2010-11-26 2:14 AM
Is there Level triger IO interrupt in Str912FAW44
2011-05-17 1:01 AM
I believe there IS a level triggered IO interrupt available, you just have to configure it through the WIU registers. There are a number of pins labeled as EXTINT in the datasheet that go to the WIU you can use. I believe there are 32 available.
Look at the WIU_TR register to set rising/falling edge sensitivity and WIU_MR to set which external interrupt lines you are interested in monitoring. Hope that helpsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.