2020-01-31 9:43 AM
Hello,
I am trying to use receive interrupts for UART0 on STR912FAW44 (STR9-Dongle STEVAL-IFD001V2)
The problem is that first few characters trasmitted to MCU don't raise receive interrupt. Then a fifth or sixth character throws receive interrupt and UART0_IRQHandler is executed (first of all trasmitted characters is echoed back to terminal). But then the MCU freezes after executing the handler. What am I doing wrong?
The code:
#include <91x_lib.h>
void SCU_init(void)
{
// Enable the UART0 Clock
SCU_APBPeriphClockConfig(__UART0, ENABLE);
// Enable the GPIO3 Clock
SCU_APBPeriphClockConfig(__GPIO3, ENABLE);
// Enable the VIC clock
SCU_AHBPeriphClockConfig(__VIC, ENABLE);
}
void uart_init(void)
{
GPIO_InitTypeDef rx_pin = (GPIO_InitTypeDef) {
.GPIO_Pin = GPIO_Pin_0,
.GPIO_Direction = GPIO_PinInput,
.GPIO_Type = GPIO_Type_PushPull,
.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable,
.GPIO_Alternate = GPIO_InputAlt1
};
GPIO_InitTypeDef tx_pin = (GPIO_InitTypeDef) {
.GPIO_Pin = GPIO_Pin_4,
.GPIO_Direction = GPIO_PinOutput,
.GPIO_Type = GPIO_Type_PushPull,
.GPIO_Alternate = GPIO_OutputAlt3
};
GPIO_Init(GPIO3, &rx_pin);
GPIO_Init(GPIO3, &tx_pin);
UART_InitTypeDef init_struct = (UART_InitTypeDef) {
.UART_WordLength = UART_WordLength_8D,
.UART_StopBits = UART_StopBits_1,
.UART_Parity = UART_Parity_No,
.UART_BaudRate = 57600,
.UART_HardwareFlowControl = UART_HardwareFlowControl_None,
.UART_Mode = UART_Mode_Tx_Rx,
.UART_FIFO = UART_FIFO_Enable,
.UART_TxFIFOLevel = UART_FIFOLevel_1_2,
.UART_RxFIFOLevel = UART_FIFOLevel_1_2
};
UART_DeInit(UART0);
UART_Init(UART0, &init_struct);
VIC_DeInit();
VIC_Config(UART0_ITLine, VIC_IRQ, 0);
VIC_ITCmd(UART0_ITLine, ENABLE);
UART_ITConfig(UART0, UART_IT_Receive, ENABLE);
UART_Cmd(UART0, ENABLE);
}
void UART0_IRQHandler(void)
{
UART_SendData(UART0, UART_ReceiveData(UART0)); // ECHO
UART_ClearITPendingBit(UART0, UART_IT_Receive);
}
int main(void)
{
SCU_init();
uart_init();
while (1) {
// Do nothing
}
}Thank you very much.
2020-01-31 10:56 AM
>>The problem is that first few characters transmitted to MCU don't raise receive interrupt.
Perhaps don't use the FIFO then? Or change the thresholds to meet your expectations.
2020-01-31 11:54 AM
Thanks for advice. When I use UART_FIFO_Disable, it raises the receive interrupt immediately after fist character sent (I propably misunderstood the FIFO concept).
But, after echoing the received character back to terminal, the MCU still keeps freezing. It just executes UART0_IRQHandler and then everything gets stuck... What can I do about that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.