2020-07-05 2:04 PM
Hi. Is there a way for an STM8 MCU to determine programmatically if the SWIM interface / ICP / STVD debugger are being used? I've tried checking the SWD bit in CFG->GCR and SWIM->CSR. But neither byte seems to change from SWIM debugging to a power on restart. The reason I ask is because an area of data EEPROM memory is always being overwritten while debugging and evidently isn't while running without STVD.
Solved! Go to Solution.
2020-07-08 3:33 PM
the answer is very simple:
2020-07-08 3:33 PM
the answer is very simple:
2020-07-08 6:18 PM
Hmm. Why the idiotic and sarcastic reply to a legitimate question, d..k? Or perhaps you're expressing some impatience with my relative nuby-iety regarding these wonderful (but somewhat complex) chips, which require a great deal of reading to understand fully, even for a dedicated engineer.
Anyway, I eventually discovered that the code was overwriting the reserved data EEPROM area without warning after a look at the MAP file. I'd just assumed (foolishly it seems) that STVD would warn me of that, since it was told specifically (via MCU Configuration) that I was using that area for data EEPROM. Yep, typical nuby mistake.
But d..k, I'm just DYING to know the answer to the three important philosophical questions you pose. Fortunately, I LIKE idiotic and sarcastic replies to legitimate questions. All the best!
2020-09-04 4:25 AM
I was wondering about the blocked flash after bootloader update.
Processor is started from powerup/reset: PUKR=0x00, IAPSR=0x40 (Flash will be open for writes after unlock)
Processor is started up from stvd: PUKR=0xAE, IAPSR=0x4A (Flash is open for write)
Processor is started up from bootloader go command: PUKR=0xAE, IAPSR=0x40 (flash is write blocked until reset)
To get the same starting condition my application starts with a reset:
if (FLASH->PUKR != 0) WWDG->CR = 0x80;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.