Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm Facing Some Serious issue on RC522 To STM32

// Waiting to receive data to complete i = 2000; // i according to the clock frequency adjustment, the operator M1 card maximum waiting time 25ms do { // CommIrqReg[7..0] // Set1 TxIRq RxIRq IdleIRq HiAlerIRq LoAlertIRq ErrIRq TimerIRq n = Read_MFR...

Major_Man_0-1710939198466.png Major_Man_1-1710939242509.png

STEVAL-SPIN3202 not driving custom BLDC motors

I am using STEVAL-SPIN3202 to drive BLDC motors other than specified in the user manual - Bull-Running BR2804-1700 kV, RS Pro 57BL54 and Faulhaber Minimotor 2036U024B. No error messages observed in ST Motor pilot. But motor does not spin.Let me know ...

sskr by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

Resolved! I/O circuit

Hey there , how can I find info to conect my STM32 with higher voltage devices , for digital inputs and outputs I have 24vcc and analogic inputs and outputs -10 to 10v, I want to conect they safely to not burn my chip.

Chris8 by Associate II
  • 5005 Views
  • 5 replies
  • 0 kudos

Resolved! UAA4003DP Chip Alternative

I am looking for a alternative chip to replace an obsolete part.The part is a ST UAA4003DP This a 16 pin chip used in a DC motor drive to control the motor speed.I can't find any information on this other than the fact that it is obsolete.. I did fin...

tsteg by Associate
  • 1687 Views
  • 2 replies
  • 1 kudos

Resolved! Info IC 902I

Hi,I can't find any information about the IC shown in the picture attached. It seems to be a very very old part that is no longer in production and ST support do not have records for anymore.Can you help find a datasheet or an equivalent component?Th...

Resolved! ECOPACK for LK115

Hi. If the device is received with no ECOPACK on packaging, does it mean it is NOT ROHS-compliant?However, datasheet says it is supposed to be in ECOPACK packages.   Is there any other way to confirm if the device is ROHS or NON-ROHS compliant?  

IReye2_0-1710334748220.png
IReye.2 by Associate II
  • 1689 Views
  • 1 replies
  • 1 kudos

Difficulty Exiting SWIM Debug Mode

Hello,I'm currently encountering an issue with my project, which is used to load .s19 files onto target devices (specifically STM8) via the SWIM protocol.Previously, the functionality was seamless when there was no external power supplied to the targ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.