2022-10-31 3:08 AM
I have a need for ST10F273MR-4Q3, but this material has been discontinued, is there a replacement for it, preferably in the same package?
Solved! Go to Solution.
2022-11-03 2:40 AM
Well, there are a very large number of potential candidates, but an exact recommendation depends very much on the peripheral units currently in use and your requirements.
If, for example, two CAN MAC are absolutely necessary, the STM32H745ZG comes into question, which otherwise offers considerably more functions and performance than the ST10F273M. It's a bit like comparing a Ford Model T with a Tesla Model Y.
For support with the redesign, I recommend contacting a local distributor.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2022-11-01 1:02 AM
Welcome, @ZJing.1, to the community!
the ST10F273M is unfortunately discontinued without replacement, there is no alternative that can be used because the technology is completely obsolete. The only remaining options:
I am sorry not to be able to give a more positive answer.
Regards
/Peter
2022-11-03 12:45 AM
Thank you for your reply
2022-11-03 12:51 AM
If the board is redesigned, what model can functionally replace it?Is there any good advice?
2022-11-03 2:40 AM
Well, there are a very large number of potential candidates, but an exact recommendation depends very much on the peripheral units currently in use and your requirements.
If, for example, two CAN MAC are absolutely necessary, the STM32H745ZG comes into question, which otherwise offers considerably more functions and performance than the ST10F273M. It's a bit like comparing a Ford Model T with a Tesla Model Y.
For support with the redesign, I recommend contacting a local distributor.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.