2010-11-12 5:33 AM
I intialize Port A3 as a push pull output but when I call writeHigh or writeLow nothing changes on that output. I am using a multimeter to read the output on pin 9 of cn1
charles2010-11-22 10:19 AM
before putting a data output on portA, you need to configure the port:
LD A, #255
LD $5002, A ;output push pull
LD $5003, A ; see page 101
brazov2
In your case , you need:LD A, #255
LD $5002, A ;output push pull
LD $5003, A ; see page 101
ld a,#4 ld $0x5000,a I don't know if are properly this value ld a,#4, Porta3 is the third 1, 2, 42010-11-22 11:33 AM
Thank you - that was it. I use 4 insted of 3
charles2010-11-23 10:51 AM
What do you mean?
Its an example, I mean If you want to get a port voltage outputs for example cn1 pin4 is ground cn1 pin9 is porta3 When you write a one in this bit, I thik you have a high output voltage between 4 and 9 you have in the multimeter screen 3,4 vdc. port a1 a2 a3 a4 a5 a6 0 0 1 0 0 0 I think you can write ld a,#4 (porta3=1) ¡¡¡Please we need a comunity expert revision data!!!2010-12-07 8:23 AM
Hi all,
even if yours is not the case, I'd like just to pay attention when using PE.2 and PE.3 port E pins, either as in or out: they're ''TRUE OPEN DRAIN''. It means that the pins don't have built-in pull-up resistors. Therefore reading in or writing out active level signals don't have effect too. In the STM8S105C datasheet page 22/127 the pin description have a small ''(T)'' aside that stands for ''True open drain''.Good work
Stefano
From: AturatePosted: Tuesday, November 23, 2010 7:51 PMSubject: IO ports
What do you mean?
Its an example, I mean If you want to get a port voltage outputs for example cn1 pin4 is ground cn1 pin9 is porta3 When you write a one in this bit, I thik you have a high output voltage between 4 and 9 you have in the multimeter screen 3,4 vdc. port a1 a2 a3 a4 a5 a6 0 0 1 0 0 0 I think you can write ld a,#4 (porta3=1) ¡¡¡Please we need a comunity expert revision data!!!2010-12-13 9:55 AM
Dear Stefano,
To obtain in cn3 pin out ''portb'' a sample example: steps of numbers from 0 to 1111111 1=3,4vcc 0=gnd with configuration needs of ddr, cr1, cr2 i have explained well? I program with asm. thank youWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.