Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The max analog sense voltage given in datasheet does not calculate correct for VND5T016ASP-E high side driver?

I am working with VND5T016ASP-E high side driver. By looking at the datasheet in current sense section, it says Vsense is tested at Iout =20A with Rsense =3.9kohm. by calculation I am not getting anywhere closer to 5V which is given as min value but ...

Bvirdi by Associate
  • 694 Views
  • 0 replies
  • 0 kudos

Receive a string 9 chars long through UART1

I would like to receive a string through the UART1, its format is from 000000000 to 999999999, However when I send the string only the first object is read and it is repeated nine times and the other values are lost.I am using this function to read t...

GGhed.1 by Associate II
  • 1783 Views
  • 2 replies
  • 0 kudos

M95M02 is no working?

Working way: W and Hold is high, Other SPI BUS.First we send "RDSR" Command but MISO is low like no working, so I try send "WREN" and "WRSR"but is no working.

0693W000001t4sVQAQ.png 0693W000001t4qPQAQ.png
Ljie.1 by Associate II
  • 1708 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.