2021-01-12 2:13 AM
I am writing a firmware for stm8 with Cosmic compiler and in ST Visual Develop. I am using astruct as the following:
typedef enum
{
lcBlack = 0,
lcRed,
lcGreen,
lcOrange
}
led_color_t;
PUBLIC typedef enum
{
lppEmpty,
lppStartup,
lpp_volt_off,
lpp_volt_warn,
lpp_volt_over,
lpp_volt_under,
lpp_volt_drop,
lppPause,
lppHY,
lppMLZ,
lppTD,
lppOnOK,
lppOff,
lppLixilTestTouch
}
led_name_t;
typedef struct
{
uint8_t enable;
led_name_t led_name;
led_color_t led_color;
uint8_t prio;
uint16_t t_on_0;
uint16_t t_off_0;
uint8_t cnt_0;
uint16_t t_on_1;
uint16_t t_off_1;
uint8_t cnt_1;
uint16_t t_1;
uint16_t t_2;
}
led_patt_t;then I define and initialize an array of structs as the following:
led_patt_t led_pattern[73] = {
{0, lppEmpty, lcBlack, 0, 0, 0, 0, 0, 0, 0, 0, 0},
{0, lppStartup, lcRed, 255, 100, 100, 10, 0, 0, 0, 0, 500},
{1, lpp_volt_off, lcRed, 210, 100, 100, 2, 0, 0, 0, 0, 1100},
{1, lpp_volt_warn, lcRed, 210, 150, 150, 2, 0, 0, 0, 0, 1300}
... }; Next I need to define a function that uses the struct array members as the following:
result_t led_pattern_request (led_patt_t led_patt){
{
led_private.pattern_current.color[0] = led_patt.led_color;
led_private.pattern_current.color[1] = led_patt.led_color;
led_private.pattern_current.priority = led_patt.prio;
led_private.pattern_current.time_on_25ms[0] = (uint8_t)led_patt.t_on_0;
.
.
.
} Where
led_data_t led_private; Then in my main I call the above function as the following:
led_pattern_request (led_pattern[17]); However, after compiling I get the follwing errors:
This is really confusing for me, I also tried to pass a pointer to the struct to the function but I get the same errors. Any help is greatly appreciated. I am new to programming and need your help.
Thank you in advance.
Best regards,
Vouria
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.