Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST M29W640FT 70N6H doubt

ST M29W640FT 70N6H flash Nor chip with 20 erase write stored in temperature 33-36C and no powered In this case, what is the most approximate and realistic estimate of years for it to retain all the information written on this chip? an approximate num...

ÍStef.1 by Associate II
  • 2146 Views
  • 3 replies
  • 0 kudos

Resolved! EVAL-RHF1201V2

Hello. im currently using the EVAL-RHF1201V2 and would like some help setting it up to properly measure dynamic characteristics. Particularly regarding the RPOL resistance and for a sampling frequency of 40 Mbps and a differential AC input from 1 MHz...

Mo9 by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! Questions about M48T201V

Hello,      I am designing with the aforementioned RTC and have the following questions.  I contacted ST support and the solution was to ask the forums.  So here are my questions:What is the date output (i.e. binary, BCD, YY:MM:DD:dd, HH:MM:SS:hh, et...

ST Micro Connection Package

We have an STMC2 in which we have lost the ST Micro Connection Package and cannot use it.Since it is obsolete in STMC2, ST does not have software. Does anyone know where I could download or buy this software?

jmartin by Associate
  • 1827 Views
  • 2 replies
  • 0 kudos

Resolved! M24512E-FMN6TP addressing

Hi,trying to get an M24512E-FMN6TP running but I only receive I2C NACKs using the default address in the DS13657 - Rev 3 - October 2023 data sheet. After some detailed reading it seems the FMN6TP device does not apply to this data sheet, there is a c...

GorEks by Associate
  • 1539 Views
  • 2 replies
  • 1 kudos

Ultra Low leakage voltage clamp

Hi everyone, I have design input protection for a CAT4 voltmeter. The Voltmeter need to measure AC+DC simultaneously. The input impedance is 10M ohm. At the moment i have an mov and a PTC as input protection that clamps at 2kv.I need some sort high s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.