2006-04-25 12:38 AM
2006-04-25 12:09 AM
Hello,
I have a numerical signal(composed of pulse of 1 and 0 logical) which arrives on the entry of the input capture of the microcontrolor st7lite It is necessary that I count the duration of the impulses which are in a high state (1) Extracts of datasheet are attached. I want to know how to measure one impulsion time with register LTICR(Life Time Input Capture Register) it is said in datasheet that we use a counter (counter 1) which counts from 0 to 255 , ther is a ltic pin which enquiries if there is a detection of a high level on the numerical signal icf flag set (1) then register LTICSR1 is containing MSB of the counter 1.But I don't understand how msb counter 1 indicates us duration of the pulse. How i Can do to know duration of the pulse with datasheet?http://shaka19free.fr/fdf/portail/upload/images/shemainputcapture.JPG
http://shaka19free.fr/fdf/portail/upload/images/counter1.JPG
http://shaka19free.fr/fdf/portail/upload/images/inputcapturetxt.JPG
________________ Attachments : counter1.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0EP&d=%2Fa%2F0X0000000bVo%2Ft0vVfikcVfdz5iBPSwcCUoTVKuXWhV0JWQa2JRHK1iI&asPdf=falseinputcapturetxt.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0EK&d=%2Fa%2F0X0000000bVm%2FojstAhLeX5YYC_A5MsrwjGGelpOzp.nGCDkMLsV6e.M&asPdf=falseshemainputcapture.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0EF&d=%2Fa%2F0X0000000bVn%2F15YTmbJLi0GVBJ.zAgn9IJjumnfFaKgSnLtZnVQRob4&asPdf=false2006-04-25 12:38 AM
Hi,
There is Application Note AN1324 available on ST web site which can help you. The method use to calibrate the RC is to measure a pulse with a known duration (50hz signal) using the input capture. This application is also available for the ST7Ultralite AN2326. Best regards LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.