2006-07-09 10:54 PM
Initialising variables after scatter loading?
2006-05-09 7:57 PM
When I run program from ram, all the variables are initialised.
When I run program after scatter loading ie: from flash, what’s copied to ram is not initialised. How do I make the variables initialised? when I boot load from flash so what copied to ram looks like initialised data?2006-05-10 6:28 PM
I figured it out, rather than using B main, I had to use B __main. It works. All the variables are initialised now.
Can some one explain the difference?2006-07-07 3:47 AM
Hello, I have the same problem.
I load code in Bank1, but when I execute it the variables don't be initialised. Where must I write ''B __main'', in 71x_init.s file? Thanks Here is my scatter file: BANK0 0x40000000 { FLASH_B0 0x40000000 ; for bank0 of internal flash { 71x_vect.o (Vect, +First) 71x_init.o (Init) * (+RO) } FLASH_B1 0x400C0000 ; for bank1 of internal flash { flash_prog.o (+RO) ; code of flash_prog file flash.o (+RO) ; code of flash file serial_flash.o (+RO) ; code of serial_flash file } RAM_0 0x20000000 ; for internal RAM { flash_prog.o (+RW,+ZI) ; data of flash_prog file flash.o (+RW,+ZI) ; data of flash file serial_flash.o (+RW,+ZI) ; data of serial_flash file * (+RW) * (+ZI) } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.