2009-07-27 9:43 PM
Indirect jump and STM8S core instruction pipeline
2011-05-17 6:03 AM
2011-05-17 6:03 AM
Hello!
the indirect jump instruction usefulness isn't clear to me. There are indeed two ways for code an indirect jump. The first one is:Code:
JP [Vector.w] while the other one is:Code:
LDW X,Vector JP (X) According to the STM8 Core Programming Manual, the former instruction is 4 bytes long and it takes 5 clock cyckes to execute. The latter two instructions take also 4 (= 3 + 1) bytes and take 4 (= 2 + 2) clock cycles to execute. I therefore see no advantage in using the indirect addressing mode because it can be emulated with index registers... How the STM8 core instruction pipeline affect my reasoning? Where can I learn more about it, since there are almost no references in the STM8 Core Programming Manual? Regards EtaPhiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.