2019-11-04 10:10 PM
#define RAM_EXECUTION (1) configured with STM8AF52xx
Use FLASH_EraseBlock in debug mode to erase normally.
In release mode (medium or high optimization) use FLASH_EraseBlock to die.
why?
2019-11-04 10:23 PM
Most probably because you use questionable constructs, or omit data/variable qualifiers.
If you e.g. not using "volatile" for externally referenced variables, the compiler will optimize it out.
2019-11-04 10:58 PM
I use STM8S_StdPeriph_Driver\src\stm8s_flash.c
IN_RAM(void FLASH_EraseBlock(uint16_t BlockNum, FLASH_MemType_TypeDef FLASH_MemType))
{
uint32_t startaddress = 0;
#if defined(STM8S105) || defined(STM8S005) || defined(STM8S103) || defined(STM8S003) || \
defined(STM8S001) || defined(STM8S903) || defined (STM8AF626x) || defined (STM8AF622x)
uint32_t PointerAttr *pwFlash;
#elif defined (STM8S208) || defined(STM8S207) || defined(STM8S007) || defined (STM8AF62Ax) || defined (STM8AF52Ax)
uint8_t PointerAttr *pwFlash;
#endif
/* Check parameters */
assert_param(IS_MEMORY_TYPE_OK(FLASH_MemType));
if(FLASH_MemType == FLASH_MEMTYPE_PROG)
{
assert_param(IS_FLASH_PROG_BLOCK_NUMBER_OK(BlockNum));
startaddress = FLASH_PROG_START_PHYSICAL_ADDRESS;
}
else
{
assert_param(IS_FLASH_DATA_BLOCK_NUMBER_OK(BlockNum));
startaddress = FLASH_DATA_START_PHYSICAL_ADDRESS;
}
/* Point to the first block address */
#if defined (STM8S208) || defined(STM8S207) || defined(STM8S007) || defined (STM8AF62Ax) || defined (STM8AF52Ax)
pwFlash = (PointerAttr uint8_t *)(MemoryAddressCast)(startaddress + ((uint32_t)BlockNum * FLASH_BLOCK_SIZE));
#elif defined(STM8S105) || defined(STM8S005) || defined(STM8S103) || defined(STM8S003) || \
defined(STM8S001) || defined (STM8S903) || defined (STM8AF626x) || defined (STM8AF622x)
pwFlash = (PointerAttr uint32_t *)(MemoryAddressCast)(startaddress + ((uint32_t)BlockNum * FLASH_BLOCK_SIZE));
#endif /* STM8S208, STM8S207 */
/* Enable erase block mode */
FLASH->CR2 |= FLASH_CR2_ERASE;
FLASH->NCR2 &= (uint8_t)(~FLASH_NCR2_NERASE);
#if defined(STM8S105) || defined(STM8S005) || defined(STM8S103) || defined(STM8S003) || \
defined(STM8S001) || defined(STM8S903) || defined (STM8AF626x) || defined (STM8AF622x)
*pwFlash = (uint32_t)0;
#elif defined (STM8S208) || defined(STM8S207) || defined(STM8S007) || defined (STM8AF62Ax) || \
defined (STM8AF52Ax)
*pwFlash = (uint8_t)0;
*(pwFlash + 1) = (uint8_t)0;
*(pwFlash + 2) = (uint8_t)0;
*(pwFlash + 3) = (uint8_t)0;
#endif
}
2019-11-04 11:36 PM
I have no experience with Flash erase/program on the STM8. Just did a project some while ago.
How about changing the optimization settings in the Debug version to medium/high, and trying to debug the issue ?
Or, instrument the Release version build (serial output or GPIO toggle) to see how far you really come.
2019-11-07 4:38 PM
Has anyone encountered a similar problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.