2023-04-16 11:16 AM
Hi Sir,
I currently use a SM6T18A/CA on the 12V+/- 5% power supply input of my product.
After this protection are located many electronic components with absolute maximum rating voltage levels (continuous) given from 13,2V to 18V.
After applying the transient voltage Test 61000-4-4 (+/-1KV levels), I can observe that one component is destroyed. I can not that it corresponds to the only component which is not HBM compliant (+-2KV).
All others components are compliant with HBM and are not destroyed even if I think the resulted clamping voltage on the SM6T18/CA regarding 61000-4-4 (+/-1KV levels) is over their absolute maximum rating voltage levels (continuous) given from 13,2V to 18V.
Thank you very much for your support.
Anthony.
Solved! Go to Solution.
2023-04-17 6:28 AM
Hi Anthony,
Thanks for sharing your case.
What is the clamping voltage level on the SM6T18A/CA regarding 61000-4-4 (+/-1KV levels)?
Is this transient clamping voltage can be considered as an issue for the electronic components after which have a maximum rating voltage level (continuous) from 13,2V to 18V?
May I consider that HBM (+/-2KV) is a guarantee to support the clamping voltage after the SM6T18A/CA protective diode (because all the current has been driven by the protective diode, and no much energy is still present on the 12V power supply rail)?
SM6T15A/CA should be better than SM6T18A/CA because :
Best regards,
Mathieu
2023-04-17 6:28 AM
Hi Anthony,
Thanks for sharing your case.
What is the clamping voltage level on the SM6T18A/CA regarding 61000-4-4 (+/-1KV levels)?
Is this transient clamping voltage can be considered as an issue for the electronic components after which have a maximum rating voltage level (continuous) from 13,2V to 18V?
May I consider that HBM (+/-2KV) is a guarantee to support the clamping voltage after the SM6T18A/CA protective diode (because all the current has been driven by the protective diode, and no much energy is still present on the 12V power supply rail)?
SM6T15A/CA should be better than SM6T18A/CA because :
Best regards,
Mathieu
2023-04-17 6:37 AM
Hi All,
This question was routed to our online support center for direct support. The above response from MROUV.1 is the direct response from the division of this request.
Regards,
Jake
ST Support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.