2017-06-13 11:42 AM
I need a simple utility to program an STM8L151G6U6TR using the USB ST-LINK V2 so that non-technical users in the field can upgrade the firmware in a consumer product. The MCU will always be STM8L151G6U6TR. So there should be no need to select an MCU. All I want the user to do is too load the s19 file and press PROGRAM. If the unit is programmed and verified correctly it would be indicated as such. That is it. No detailed information should be displayed, no code detail or any other info.
2017-06-14 6:16 AM
ST maintains a list of consultants and contractors who might be able to assist with your coding task.
http://www.st.com/en/development-tools/stvp-stm8.html
2017-06-14 10:28 AM
Clive,
I do not see the list of consultants. Please point me to the link.
Thanks
2017-06-14 10:53 AM
http://www.st.com/content/st_com/en/support/partners/design-consultants-for-mcus.html
Your FAE (via ST or Distributor) might also have some ideas, suggestions or experience.
This type of 'simple' in my experience is quite complicated (time consuming) to achieve.
2017-07-03 12:53 AM
It would be easy to add the desired simple user interface on top of stm8flash (assuming the users are running GNU/Linux - I don't know how much effort it would be to port stm8flash to other OSes):
https://github.com/vdudouyt/stm8flash
Philipp
2017-07-03 10:38 AM
The program utility has to work with Windows only, no other OS. Please keep in mind that I am not a software engineer (hardware only), but it seems that STM32 STLINK Utility should work using command line interface. However, I cannot connect to the target at all with the utility or the CLI. The only way I can repeatedly program the STM8L15 is via the STVP.exe. If I can get it to connect to the target, then the CLI would allow a simple programming script I would think.
2017-07-03 12:11 PM
I just found out that the STM32 STLINK utility is not compatible with STM8. I am going to try the CLI utility that comes with the STVP package.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.