2007-03-27 11:34 PM
2011-05-17 12:40 AM
Hi,
I tried to use external interrupts but it doesnt work. Im using the mcbstr9 eval board vers. 4 from keil. Here is my code:Code:
<BR> <BR>__irq void EXT_WIU1_IRQ_Handler(void); /* EXT interrupt routine */ <BR>int count = 0; <BR> <BR>int main(void) <BR>{ <BR> <BR> SCU->GPIOIN[5] = 0x00; /* P5.0..7 input - mode 0 */ <BR> SCU->GPIOOUT[5] = 0x0000; /* P5.0..7 output - mode 0 */ <BR> GPIO5->DDR = 0x00; /* P5.0..7 direction - input */ <BR>//SCU->WKUPSEL = 0x0038; /* use P5.7 as VIC1.11 interrupt src*/ <BR> <BR> /* Configure and enable IRQ for EXTINT WIU Group 1 */ <BR> VIC1->VAiR[11] = (unsigned int)&EXT_WIU1_IRQ_Handler; <BR> VIC1->VCiR[11] |= 0x20; /* Enable the vector interrupt */ <BR> VIC1->VCiR[11] |= 11; /* Specify the interrupt number */ <BR> VIC1->INTSR &= ~(1<<11); /* Set Interrupt as IRQ */ <BR> VIC1->INTER |= (1<<11); /* Enable EXT interrupt */ <BR> <BR> <BR> <BR> while(1) <BR> { <BR> <BR> /* some code to print variable 'count' */ <BR> <BR> } <BR>} <BR> <BR> <BR> <BR>__irq void EXT_WIU1_IRQ_Handler(void) /* EXT interrupt routine */ <BR>{ <BR> count++; <BR> <BR> VIC0->VAR = 0; /* Acknowledge Interrupt */ <BR> VIC1->VAR = 0; /* Acknowledge Interrupt */ <BR>} <BR>
GPIO5 uses external interrupts 8 to 15 as default input function. They are grouped to WIU group 1 and is connected to VIC1.11. I also tried to mask one of GPIO5 bit in SCU->WKUPSEL, but the interrupt routine is never called. any ideas? [ This message was edited by: MarcoHansen on 26-03-2007 20:42 ]2011-05-17 12:40 AM
HI
You can use only one of the 8 pins of GPIO5 as external interrupt. for the code u hav shown atleast one pin should hav worked bye2011-05-17 12:40 AM
Hi,
I already tried to use P5.7 as intterupt source but it doesnt work.2011-05-17 12:40 AM
Hi,
Did u set up the WIU registers? Enable the WIU interrupt in WIU->CTRL and WIU->MR registers Also u may have to set the pin as alternate input 1 in the GPIOIN register...2011-05-17 12:40 AM
Hi,
I tried these config:Code:
WIU->CTRL |= 0x02; /* Global WIU Interrupt enable */ WIU->MR |= 0xFFFC; /* Enable all Interrupts in Maskreg */ No effect. Setting the input as alternate input also has no effect.2011-05-17 12:40 AM
Hi,
I added these lines:Code:
SCU->PCGRO |= (1<<5); /* Enable VIC peripheral clock gating*/ SCU->PCGR1 |= (1<<19); /* Enable GPIO5 port clock gating */ SCU->PCGR1 |= (1<<13); /* Enable WIU peripheral clock gating*/ SCU->PRR0 |= (1<<5); /* VIC not held in reset */ SCU->PRR1 |= (1<<19); /* GPIO5 not held in reset */ SCU->PRR1 |= (1<<13); /* WIU not held in reset */ Also no effect. The output of GPIO5-register shows change of value so input should work correctly.2011-05-17 12:40 AM
Hi,
Did u enable the clock gating and disable the reset for the VIC, WIU and GPIO peripherals?2011-05-17 12:40 AM
This works for me:
Code:
WIU->PR = 0xFFFFFFFC; // Clear pending interrupts WIU->MR = WIU_Line2; // Enable external interrupt from pin3_2 (interrupt pin) WIU->CTRL = WIU_Mode_Interrupt; // Enable interrupt from pins VIC1->VAiR[9] = (unsigned int)interrupt_handler; // Setup external interrupts handler vector VIC1->VCiR[9] = 0x20; // Enable the vector interrupt VIC1->VCiR[9] |= (WIU_ITLine-16); // Specify the interrupt number VIC1->INTER = (1 << (WIU_ITLine-16)); // Enable interrupt I use VIC1.9 and pin 3.2 for external interrupt... The predefined numbers are from the ST library header files...2011-05-17 12:40 AM
Hi,
I tried your code, but it doesnt work. I had to set up the port clock gating in startup code. Writing to SCU->PCGR1 had no effect. I attached the project. Maybe I forgot something to configure in startup code or there is something wrong with the board. :-?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.