2007-03-26 2:26 AM
2011-05-17 12:40 AM
If I don't set the WSR_AHB bit in SCR0, memory to memory DMA never finish! (it never starts)
WSR_AHB: AHB Wait state enable This bit is set and cleared by software to enable/disable the insertion of a wait state during an SRAM read access performed on the AHB bus 0: No wait state 1: 1 wait state (default) Like the SRAM arbiter don't let the DMA to access the AHB! Is this a normal behavior? I'm runing at 96 MHz. What should I read to understand how these setting influence system performance? Less wait-states should be better ? WSR_AHB,WSR_DTCM are set by default and usually startup files leave them in 1. It may because of this? thanks, AndrasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.