2021-06-03 9:54 PM
Hi,
I want to run STM8S003F with an external crystal.
How do I use APIs in stm8_clk?
Or in which material is it described?
Regards,
Gotoda
Solved! Go to Solution.
2021-06-10 1:05 AM
So you see a signal on CLK_CCO. That means that either the crystal oscillator or the internal RC oscillator is functional. Since you see a 2 MHz signal that suggests that it is the internal RC oscillator, as by default its 16 MHz freq is divided by 8. And you do not divide the CLK_CCO signal. The odd thing is that you select HSE as the CLK_CCO signal, that doesn't make sense.
Can you give the code below a try? It works for me, although I did not have a 16 MHz crystal, but used an 8 MHz one.
The oscilloscope shows a (small) 8 MHz signal on both PA1 and PA2, Make sure to use a probe that doesn't load the oscillator too much (10x probe)
void HSE_config(void)
{
CLK_DeInit();
CLK_HSECmd(ENABLE);
CLK_LSICmd(DISABLE);
CLK_HSICmd(DISABLE);
while(CLK_GetFlagStatus(CLK_FLAG_HSERDY) == FALSE);
CLK_ClockSwitchCmd(ENABLE);
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE,
DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
}
void CLOCK_output(void)
{
CLK_CCOConfig(CLK_OUTPUT_CPUDIV8);
CLK_CCOCmd(ENABLE);
while(CLK_GetFlagStatus(CLK_FLAG_CCORDY) == FALSE);
}
2021-06-03 11:54 PM
The first resources to read are the RM0016 reference manual, where to search for HSE (High-Speed External Oscillator), and the STM8S003 datasheet.
Then check the Standard Peripheral Firmware Library (SPL) STSW-STM8069, which contains some user manual, describing the function to enable the HSE. And finally you can also check this SPL for the files stm8s_clk.c and stm8s_clk.h, where you will find the function CLK_HSECmd(ENABLE).
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-06-04 12:37 AM
Also read application note AN2752, It even has a reference Design (chapter 7)
2021-06-07 6:35 PM
I implemented the following code to see if the external clock works, but I couldn't observe the clock.
void main(void)
{
CLK_DeInit();
CLK_HSECmd(ENABLE);
while(1);
}Are there any missing implementations or configs?
2021-06-09 5:41 PM
When implemented as follows, it was confirmed that 2MHz was output from the PC4 (CLK_CCO) terminal, but no clock waveform was observed at the OSCOUT terminal.
void main(void)
{
CLK_DeInit();
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
CLK_HSECmd(ENABLE);
CLK_ClockSecuritySystemEnable();
CLK_CCOConfig(CLK_OUTPUT_HSE); //View output via PC4
CLK_CCOCmd(ENABLE);
while(1);
}I checked the voltage waveforms of OSCOUT and OSCIN with an oscilloscope, but I could not observe 16 MHz.
I am using a 16MHz xtal with 12pF capacitors and 0 ohms resistor.
How can I code this crystal to oscillate?
2021-06-10 1:05 AM
So you see a signal on CLK_CCO. That means that either the crystal oscillator or the internal RC oscillator is functional. Since you see a 2 MHz signal that suggests that it is the internal RC oscillator, as by default its 16 MHz freq is divided by 8. And you do not divide the CLK_CCO signal. The odd thing is that you select HSE as the CLK_CCO signal, that doesn't make sense.
Can you give the code below a try? It works for me, although I did not have a 16 MHz crystal, but used an 8 MHz one.
The oscilloscope shows a (small) 8 MHz signal on both PA1 and PA2, Make sure to use a probe that doesn't load the oscillator too much (10x probe)
void HSE_config(void)
{
CLK_DeInit();
CLK_HSECmd(ENABLE);
CLK_LSICmd(DISABLE);
CLK_HSICmd(DISABLE);
while(CLK_GetFlagStatus(CLK_FLAG_HSERDY) == FALSE);
CLK_ClockSwitchCmd(ENABLE);
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE,
DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
}
void CLOCK_output(void)
{
CLK_CCOConfig(CLK_OUTPUT_CPUDIV8);
CLK_CCOCmd(ENABLE);
while(CLK_GetFlagStatus(CLK_FLAG_CCORDY) == FALSE);
}
2021-06-11 12:21 AM
I can't get out of the CLK_GetFlagStatus() loop.
CLK_ECKR value is 0x01 (HSE clock on but not ready).
CLK_ICKR is 0x03.
Is there a hardware (our custom board) cause?
2021-06-13 2:37 AM
It means that you enabled power to the HSE, but it isn't oscillating. And because you had the line
CLK_ClockSecuritySystemEnable();in your code, the MCU switched back to the HSI.
So yes it looks like there is something wrong with the hardware, perhaps a crystal that is broken. Have you tried replacing it? Are the capacitors of the right value?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.