2020-09-15 6:08 AM
I need to decode ASK/OOK signal, for this aim I need to know the period in microseconds between several edges. I decided to use TIM1 for this purpose, here is my code
// Set fCPU = 16MHz
CLK_CKDIVR = 0;
CLK_PCKENR1 = 0xFF;
CLK_PCKENR2 = 0;
uint16_t micros() {
return (uint16_t) ((TIM1_CNTRH << 8) | TIM1_CNTRL);
}
void tim1_init(void) {
// 1MHz = 1uS
TIM1_PSCRH = 0x00;
TIM1_PSCRL = 0x10;
TIM1_IER = 0x00; // disable interrupts
TIM1_CR1 = 0x01;
}and to get signal I use
ISR_PORTD(handlerD) {
state = PinRead(GD0_PORT, GD0_PIN);
uint16_t m = micros();
if (state == HIGH) {
lolen = abs(m - prevtime);
}
else {
hilen = abs(m - prevtime);
}
prevtime = abs(m);
if (state == HIGH)
{
if (flag == 0) {
// the end of packet
if (CheckValue(Pe, hilen) && CheckValue(Pe2, lolen)) // valid 1
{
if (bcounter < 32)
code1 = (code1 << 1) | 1;
else if (bcounter < 64)
code2 = (code2 << 1) | 1;
bcounter++;
}
else if (CheckValue(Pe2, hilen) && CheckValue(Pe, lolen)) // valid 0
{
if (bcounter < 32)
code1 = (code1 << 1) | 0;
else if (bcounter < 64)
code2 = (code2 << 1) | 0; bcounter++;
}
else
bcounter = 0;
}
else {
if (bcounter < 32)
code1 = (code1 << 1) | 1;
else if (bcounter < 64)
code2 = (code2 << 1) | 1;
bcounter++;
}
}
//printf("bcounter: %d\r\n", bcounter);
if (bcounter >= 65)
{
printf("Got: %x %x\r\n", code1, code2);
Pe2 = lolen;
Pe = hilen;
flag = 1;
bcounter = 0;
code1 = 0;
code2 = 0;
}
}but get the values not I expected
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.