2023-02-01 2:47 AM
Hello everyone !
I created a design based on this board from TI : TIDA-00325
The goal is to create board converting a HDMI input in another format. I'm not really familiar with the HDMI protocol but it seems an EEPROM is often used with it, that's why I chose the M24C02-WMN6TP.
I would like to know how this component is configured, do I need to configure it myself before or will it work just by connecting it on the I2C bus (already connected to the ITE6801FN and the HMDI port) ?
Since english is not my first language, let me know if you want me to rephrase it or if I need to give further information.
Best regards,
Romain.
Solved! Go to Solution.
2023-02-01 4:41 AM
Welcome, @Romain Quesada, to the community!
Well, an EEPROM like the M24C02-WMN6TP is a non-volatile memory where data is stored, which normally does not require configuration.
However, if the IT6801FN needs a pre-configuration from the EEPROM for its work, you have to ask the manufacturer of the IT6801FN.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-02-01 4:41 AM
Welcome, @Romain Quesada, to the community!
Well, an EEPROM like the M24C02-WMN6TP is a non-volatile memory where data is stored, which normally does not require configuration.
However, if the IT6801FN needs a pre-configuration from the EEPROM for its work, you have to ask the manufacturer of the IT6801FN.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-02-02 5:42 AM
Thank you for your time and have a nice day !
Romain.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.