2010-08-12 4:34 AM
How Take string from web form to cgi-function?
2011-05-17 1:01 AM
In httpd.c by Adam Dunkels I found that:
/* We use the uip_ test functions to deduce why we were called. If uip_connected() is non-zero, we were called because a remote host has connected to us. If uip_newdata() is non-zero, we were called because the remote host has sent us new data, and if uip_acked() is non-zero, the remote host has acknowledged the data we previously sent to it. */ if(uip_connected()) { /* Since we have just been connected with the remote host, we reset the state for this connection. The ->count variable contains the amount of data that is yet to be sent to the remote host, and the ->state is set to HTTP_NOGET to signal that we haven't received any HTTP GET request for this connection yet. */ hs->state = HTTP_NOGET; hs->count = 0; Where (In what variable) can I found string sending to server by method ''GET'' of WebForm? I need to get vaues of form's tags SELECT and INPUT type=checkbox. Thank you.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.