2006-05-08 11:42 PM
2006-05-08 9:19 PM
hello,
i would like to configure the P1.11 as external interrupt. how do you it? It is possible to show me what register are configured to use correctly this pin. thanks Ludovic2006-05-08 11:42 PM
Hi
Some ports (like P1.11) have external interrupt capability . To use external interrupts, the port must be configured in input mode. Each of the General Purpose I/O Ports has three 16-bit configuration registers (PC0, PC1,PC2) and one 16-bit Data register (PD). You can refer to the STR71x Ref Man for more details. Regards, HichWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.