2006-05-08 11:09 PM
2006-05-05 12:46 AM
I am using st72f561 with cosmic compiler & STVD7 environment. I want to use global bit variables, hence I have edited the Linker file & it looks like this,
+seg .text -b 0x1000 -m 0xD000 -n .text +seg .const -b 0xE000 -m 0x200 -n .const +seg .bit -b 0x0080 -m 0x10 -n .bit -c +seg .bsct -b 0x0090 -m 0x50 -n .bsct +seg .ubsct -b 0x00E0 -m 0x1F -n .ubsct +seg .share -a .ubsct -n .share -is +seg .data -b 0x0200 -m 0x600 -n .data +seg .bss -a .data -n .bss The default linker file did not contain .bit segment, so I added the segment in the linker file. The compile, Build, Link went correct, w/o any error or wanrning. The bit started behaving randomly, hence I checked the map file. The map file was showing that it was mapped at the address of PFDDR:0. How to avoid the problems related to globally declared bits?? At the same time, localy declared bits are working properly & they were not visible in the map file.2006-05-05 2:37 AM
2006-05-08 3:44 AM
Thank you Luca :)
We did the changes in the linker file as per suggested by you. The results are very good. The global bit is mapped exactly at 000080:0 & serving it's purpose perfectly. Thank you again. Can you guide us towards any such document, in which such Compiler & Linker details are mentioned. We want to study this bit segemnt issue in detail to find out, where we went wrong in our approch to edit the linker file for the bit segment. Regards, Yogesh & Amit2006-05-08 11:09 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.