2020-12-10 4:24 AM
From the point of view of firmware in microcontroller, which is communicating with STUSB4500 by I2C, how can it find out what PDO (voltage and current) has been negotiated with the power source.
I am particularly interested in maximum current so the microcontroller can ensure it doesn't exceed this.
2020-12-10 3:26 PM
Hi,
With STUSB4500, To get the PDOs available on the Source side, you can use the GetSrcCap() function.
Get Source Capabilities :
https://github.com/usb-c/STUSB4500/blob/master/Firmware/Project/Src/USB_PD_core.c#L1124
The PDO that has been negociated between the USB-C Sink and Source is called RDO = Request Data Object
To get the RDO, you can use the Print_RDO() function:
https://github.com/usb-c/STUSB4500/blob/master/Firmware/Project/Src/USB_PD_core.c#L541
Regards
2020-12-11 12:28 AM
Thanks for your reply Gregory.
The value in RDO is sometimes correct, but sometimes it reports 22.5V when I have requested 20V (and VBUS is at 20V):
STUSB regs:
00: 0x12 0x00
08:0x11 0x20 0x00 0x01 0xF9 0x00 0x41 0x00
10:0x0A 0x13 0x00 0x40 0x00 0x02 0x00 0x2C
18:0x00 0x00 0x26 0x21 0x01 0x80 0x00 0x00
20:0x10 0xC8 0x5F 0x00 0x00 0x9C 0x00 0x02
28:0x02 0x18 0x00 0xE1 0x05 0x00 0x00 0x21
30:0x00 0x66 0x07 0x7D 0x4B 0x1A 0xEC 0xC0
38:0xA1 0x05 0x00 0xC2 0x41 0x06 0x00 0x25
40:0xBE 0xA1 0x80 0x00 0x00 0x00 0x00 0x00
48:0x00 0x00 0x00 0x00 0x00 0x18 0xE3 0x00
50:0x00 0x0D 0x00 0x00 0x4B 0x2C 0x21 0x43
58:0x00 0x48 0xFB 0x00 0x00 0x00 0x00 0x00
60:0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
68:0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
70:0x43 0xC8 0x90 0x01 0x08 0x64 0xD0 0x02
78:0x00 0x2C 0xB1 0x04 0x00 0xF4 0xB1 0x04
80:0x00 0x5E 0xFD 0x01 0x00 0x96 0x90 0x01
88:0x10 0xC8 0xB0 0x04 0x00 0xC2 0x41 0x06
90:0x00 0xC2 0x09 0x07 0x30
DPM_SNK_PDO1(Pdo 10019096 fix mV=5000 mA=1500)
DPM_SNK_PDO2(Pdo 0004B0C8 fix mV=15000 mA=2000)
DPM_SNK_PDO3(Pdo 000641C2 fix mV=20000 mA=4500)
DPM_REQ_RDO (Pdo 300709C2 fix mV=22500 mA=4500)
2021-01-05 5:28 PM
Be careful that the Source Capabilities PDOs are available in STUSB4500 registers only for a short time (few ms) , until the next USB PD message from the Source overwrites the buffer with new data.
So if you read an incorrect value like 22.5V, it means you have missed the right USB-PD message. Thus you should try again.
2021-01-06 12:08 AM
Thanks Gregory.
Yes, I found that reading the message header and data (from address 0x31 ...) needs to be done quickly (before the next message overwrites it).
But I am seeing strange values at DPM_REQ_RDO (address 0x91 ...0x94) (see register dump above).
Is there any reason why the data address would not be valid ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.