2006-09-21 11:53 PM
2011-05-17 12:30 AM
Hi:
I wrote a simple example to test the maximum speed of the GPIO. All I did was toggle the GPIO pin between 0 and 1. The maximum speed at which the pin was toggling was 400Hz when the MCLK is 32 KHz (RTC oscillator). The code for this example is: SCU_MCLKSourceConfig(SCU_MCLK_RTC); for(i = 0; i< 100; i++); SCU_PLLCmd(DISABLE); SCU_RCLKDivisorConfig(SCU_RCLK_Div1); SCU_HCLKDivisorConfig(SCU_HCLK_Div1); SCU_PCLKDivisorConfig(SCU_PCLK_Div1); SCU_APBPeriphClockConfig(__GPIO4,ENABLE); SCU_APBPeriphReset(__GPIO4,DISABLE); while(1){ *(u8 *)0x5800A010 = 0x00; *(u8 *)0x5800A010 = 0x04; } It’s quite slow to my expectations. Any pointers on this problem would be appreciated. Regards,2011-05-17 12:30 AM
Hi Iamanil,
the two code lines inside the while loop takes many cycles, so that the GPIO speed will be quite slow. However if you select the maximum optimization of the IAR tool your disassembly code will be as follow: STR R4, [R0, #+0] STR R6, [R0, #+0] B 0x000CA4 In this case of optimization, frequency can reach 1.168 KHz. We can even reach 2.717KHZ if we use the Buffered mode: that means code will be: while(1) { *(u32 *)0x4800A010 = 0x04; *(u32 *)0x4800A010 = 0x00; } Regards.2011-05-17 12:30 AM
Hi eris,
I am first time using ARM9. Do you do the same test when running the MCU under the PLL mode (96MHz), and what is your results? Does it able to perform 96MIPS? RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.