2008-10-08 8:54 PM
2011-05-17 12:51 AM
Now I run PLL at 96MHZ PLL and FLASH at 48MHZ, when I set one GPIO from
0->1->0, it takes about 400ns... is it normal? But if I calculate the ideal speed of it, it should be less than 50ns, right? Because I need to use GPIO to simulate parallel port data/address... now the actual speed of GPIO is too slow... Is anyone know how to improve it? Please kindly give me advices. Thank you very much.2011-05-17 12:51 AM
Hi
See: '' TARGET=''_blank''> > 6MHz square wave (12MHz toggle)is achievable. Regards Mark2011-05-17 12:51 AM
Hello,
I develop an application with the STR9-Comstick. The idea is to control the I/O ports with a program in Visual Basic through the USB-B connector near the pins of I/O ports. Which dll use for that for the enumeration ? The first application will be to generate a TTL signal for differents frequencies through a pin of the I/O ports. Is there a way to program it in C (TTL signal) for the STR9 ? And so the program in VB ? Regards Vlieghe GuillaumeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.