2026-03-19 4:08 AM - last edited on 2026-03-19 4:39 AM by mƎALLEm
Split from USART in Proteus not displaying any characters as this is now a new situation (real hardware; not simulation)
Now as per your advise i have moved from simulation to real hardware can you please why under freertos its not working the led is counitnusly onn instead of blinking?
Working behavior:
LED blinks correctly without FreeRTOS using a simple while loop in the same setup .
Flashing and debugging via ST-LINK works without issues.
Problem:
When FreeRTOS is enabled, the LED stays continuously ON instead of blinking under the same hood .
CubeMX configuration:
FreeRTOS enabled (CMSIS V2)
Default task created
USE_NEWLIB_REENTRANT enabled in FreeRTOS advanced settings
SYS timebase tested with:
SysTick
TIM1
GPIO PC13 configured as:
Output ( that is fine as it worked without freertos but stays counitnuoly on with freertos )
Code behavior:
Using osDelay() inside the task
Same toggle logic works outside FreeRTOS but not inside
What I have tried:
Switching between SysTick and TIM1 timebase
Re-generating code multiple times
Verifying task loop logic
Replacing HAL_Delay with osDelay
Question:
Why does the LED remain ON when FreeRTOS is enabled instead of blinking can you please check configurations for freertos ?
Is this related to timebase configuration, scheduler issue, or HAL vs RTOS conflict?
What am I missing in my configuration ?I m so confused here why it might beahvees like this i have attached the project folder can you please check this and inform where is an actual issue underlying?
Any help or suggestions would be appreciated. Thank you.
Solved! Go to Solution.
2026-03-19 4:38 AM - edited 2026-03-19 4:43 AM
As stated by the OP in this post, he's using a Blue Pill board.
As ST we cannot help on that.
I suggest you to purchase a ST board with a genuine chip for example NUCLEO-F103RB, so we will happy to help you.
Thank you for your understanding.
2026-03-19 4:17 AM
@Muhammad_Umer_Asif wrote:i have moved from simulation to real hardware
So what hardware are you using ?
How to write your question to maximize your chances to find a solution
What debugging have you done ?
Is your code which blinks the LED ever getting called ?
2026-03-19 4:38 AM - edited 2026-03-19 4:43 AM
As stated by the OP in this post, he's using a Blue Pill board.
As ST we cannot help on that.
I suggest you to purchase a ST board with a genuine chip for example NUCLEO-F103RB, so we will happy to help you.
Thank you for your understanding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.