Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STi7101 Board Support Package

Dear STMicroelectronics Community, I am an electronics engineer seeking for technical help. My problem is that I want to reverse engineer an old STi7101 CPU based Set Top Box with HDMI output or say it less complicated, a Dish Antenna Receiver Box. M...

MrArnold by Associate
  • 244 Views
  • 1 replies
  • 0 kudos

Resolved! FIT rates: STM32C092GCU6 & LIS2HH12TR

Dear ST Support Team,I am working on a reliability calculation for an industrial hardware design. I need the official failure rate data for the following components:STM32C092GCU6: FMEDA report and FIT rates LIS2HH12TR: Reliability report and FIT rate...

Unit Testing tool recommendation?

Hello! I’m aware that the question I’m asking may have many correct answers since everything depends on the application and specific needs, but I’d like to know which Unit Testing tool you recommend. Ideally one that is easy to use, adapts well to di...

STSPIN32G4 VDS failure

Hello, When using the STSPIN32G4 to drive a three-phase bridge for BLDC control, the MOE pin is automatically set to 0. Reading the internal driver status register of the STSPIN32G4 shows the VDS bit is set to 1. I have already set a sufficiently hig...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.