2011-03-20 8:20 AM
Hi, I have problem with IAR and Downloading files to FLASH memory. Yesterday was everything allright but today when I wanted download my code to FLASH, it was impossible and still is...
This is in my debug log: Sun Mar 20 15:57:50 2011: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\config\flashloader\ATMEL\resources\ FlashAT91SAM7Sxx.mac Sun Mar 20 15:57:50 2011: Sign on message from : Remote Debugging Interface for JTAG in-circuit debugging Sun Mar 20 15:57:50 2011: ---------------------------------------- FLASH Download V1.3 Sun Mar 20 15:57:50 2011: ---------------------------------------- 14/November/2005 Sun Mar 20 15:57:50 2011: ---------------------------------------- PLL Enable Sun Mar 20 15:57:50 2011: -------------------------------Set CPSR ---------------------------------- Sun Mar 20 15:57:50 2011: CPSR 000000D3 Sun Mar 20 15:57:50 2011: ---------------------------------------- PLL Enable Sun Mar 20 15:57:50 2011: ------------------------------- The Remap is NOT ----------------------------------------- Sun Mar 20 15:57:50 2011: ---------------------------------------- Chip ID 0xFFFFFFFF Sun Mar 20 15:57:50 2011: ---------------------------------------- Extention 0xFFFFFFFF Sun Mar 20 15:57:50 2011: ---------------------------------------- Flash Version 0xFFFFFFFF Sun Mar 20 15:57:50 2011: -------------------------------Set PC ---------------------------------------- Sun Mar 20 15:57:51 2011: 6656 bytes downloaded and verified (6.94 Kbytes/sec) Sun Mar 20 15:57:51 2011: Warning: Target inconsistency detected in Memory range 0x00000000-0x000019FF Sun Mar 20 15:58:05 2011: Fatal error: There were warnings during download of FLASH loader, see Log Window Session aborted! Sun Mar 20 15:58:05 2011: Failed to load flash loader: C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\config\flashloader\ATMEL\ AT91SAM7S64-EK\internalflash-sam7s64.out Sun Mar 20 15:58:05 2011: Failed to load flash loader: C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\config\flashloader\Atmel\ AT91SAM7S64-EK\flash-at91sam7s64.flash Pls, what can I do ? Thanks for helps. P.2011-03-28 11:03 AM
Sun Mar 20 15:57:50 2011: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 5.4\arm\config\flashloader\ATMEL\resources\
FlashAT91SAM7Sxx.mac
Yeah, well using a ATMEL flash template is a sure fire way to fail on an STMicro part. Make sure you're picking the right target CPU, and have the right flash memory setup.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.