2020-04-15 1:51 PM
Hello
I wonder if there is some example code available on how to use the Data EEPROM in the 8pin STM8L001J3.
I did successfully work with the internal Data EEPROM on the STM8L051, but no success on the SO8. The address I used is 0x9BFB (in contrast to 0x1000 on the STM8L051). There is no error when debugging the code in ST Visual Develop/Cosmic, but the content of the bytes I want to alter does not change.
Best regards
Thomas
2020-04-20 7:37 AM
TO WHOM IT MAY CONCERN:
Unlike all official examples show and all documentation implies, it is needed to address the Data EEPROM as if it was Program EEPROM. Hence the following code works:
// Do this once, e.g. after power-up:
FLASH_DeInit();
FLASH_SetProgrammingTime(FLASH_ProgramTime_Standard);
// Do this for each write access
// Unlock the Flash
FLASH_Unlock(FLASH_MemType_Program);
// copied from FLASH_ProgramWord: "Enable Word Write Once"
FLASH->CR2 |= FLASH_CR2_WPRG;
// Do what you need, e.g.
FLASH_ProgramByte(EEPROMSTARTADDR, "yourDataByte");
// ...
// Finalize
FLASH_Lock(FLASH_MemType_Program);
"EEPROMSTARTADDR" in my case is #defined as 0x9FC0
Best regards
Thomas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.