Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD, docking windows in debug mode

Hello,Tell me how to pin windows such as Local Variables, Peripheral Registers, Memory in debugging mode in STVD? (When you enter debug mode, you need to open these windows manually; the next time you enter debug mode, these windows disappear and you...

MykolaLevun_0-1705679538190.png MykolaLevun_1-1705679627809.png

DAC in MCP2221

Hi to all!I am trying to generate an analog signal using a DAC that is built into the MCP2221 controller. The problem is how do I control the output current? Maybe there are some schemes or built-in capabilities in the MCP2221 controller? Is it enoug...

Watchdog Timer application

Hello Team,We are considering STM6822SWY6F Watchdog IC for our design.We have query regarding WDI input pulse for time out condition. What is status of Reset pin, if WDI pin is fixed to High or Low voltage level even after 1.6 sec of time out period?...

kadam by Associate II
  • 2163 Views
  • 3 replies
  • 0 kudos

Inbuild filtering of iNEMO inertial module

Hi, I am using LSM6DSO IMU sensor to track motion and need to know the specifications of the inbuild Low pass filters. Datasheet only shows the block diagram and does not provide any information about filter type, order, frequency response. Could you...

Screenshot 2024-01-18 100714.png
zce by Associate
  • 1002 Views
  • 0 replies
  • 0 kudos

STM8 UART

I am frustated from last month can anyone plz help me outI am getting error if I am adding UART file in our program.I have taken UART example provided in STM8S_StdPeriph_Examples and added those files in STM8S_StdPeriph_Template but without adding UA...

Pankaj3 by Associate II
  • 2931 Views
  • 4 replies
  • 1 kudos

STM8 SPBTLE-RF bluetooth communication problem

Hello everyone, i've an issue using STM8L with an SPBTLE-RF bluetooth module.It seems that the module stop to transmits data to the master after few time of utilization or during an intensive use.I verified that when the module stop to transmits data...

Alberto3 by Associate
  • 1241 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.