2020-02-11 4:45 AM
Hello friends,
We use ST-Link when assigning programs to STM8 processors. ST-Link uses the SWIM leg when assigning programs to STM8 processors. We all know that.
I want to make a device. Special bootloader. This device should be able to assign programs to STM operators that do not have programs in the device.
But I don't have a protocol to throw a program into the empty processor. Is there such a protocol? Is such a device possible? Where can we obtain a protocol?
Thanks, good work ..
2020-02-11 4:51 AM
> We use ST-Link when assigning programs to STM8 processors. ST-Link uses the SWIM leg when assigning programs to STM8 processors.
Your terminology is ... peculiar. Googel-translate ?
There is a multitude of threads regarding custom bootloaders on this forum, mainly the STM32 section.
A custom Bootloader is basically a normal application that two things:
-> jump to a present main application; or
-> load updates, and program (Flash) them;
2020-02-11 5:31 AM
Sorry, yeah google-translate :)
I made a custom bootloader before. I want to make a device like st-link.
2020-02-11 5:35 AM
So, something like this: http://openocd.org/
2020-02-11 6:09 AM
Thank you for sharing link..
Yes, like this. But something simpler is what I want to do.
For example, to program the processor with st-link,
> We upload the hex file to the STVP program.
> Then we send the program to the processor by pressing the relevant button.
It is easy to send the program uploaded to STVP to the st-link device.
What I really want to reach is what kind of protocol it is when assigning a program from the st-link to the processor.
So how is it programmed with SWIM pin even though there is no program in the processor? It is clear that there is a protocol. But where?
2020-02-11 6:17 AM
I don't know ST's SWIM interface/protocol in detail. Most probably a proprietary hardware/protocol, before the advent of JTAG.
Cortex M use JTAG, it a reduced version named SWD. It operates on hardware on the target, which operates in parallel and independant of the core itself.
And it is usually everything else but simple.
2020-02-11 6:23 AM
You mean like a stand alone production programmer?
https://www.segger.com/products/production/flasher-st/models/flasher-stm8/
2020-02-11 9:36 AM
I understand. Thank you for reply..
2020-02-11 9:38 AM
Yes, I want to make a similar device. No need to debug. It is enough to program the processor.
But I do not know exactly how to proceed.
2020-02-11 10:07 AM
Contact local ST sales/support and see if you can get the protocol documentation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.