2019-09-11 12:45 AM
I'm sorry, I'm not a STM8 developer
I just want to upgrade an RFID reader
The CPU is STM8S003F3
The programmer is ST-LINK V2
The connection is SWIM
The programmer is ST Visual Programmer
It gives me the error "The device is protected"
Is there any way to erase everything to update the firmware?
2019-09-12 7:29 AM
Hi!
Any MCU out there should be protected. The STM8 has a so called Read-Out Protection mechanism.
In order to disable the read out protection, you only need to program the ROP option byte to a value different than 0xAA, normally 0x00 (the programmer should have a special command for this, like unlock device or so).
Through this operation the device will erase itself, so make sure you have the right firmware to write back.
Good luck!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.