2008-09-08 7:33 AM
2011-05-17 12:55 AM
With the below piece of code, i am able to generate an interrupt at every
0.35sec (350msec). 1. Can anyone tell how this stuff works? 2. Also, I want to change a little bit this code and generate an interrupt at my own specified msec? Thanks in advance, Thanga /***********************************************************************/ #define WDG_ClockSource_Apb 0xFFFB /*The APB clock signal will be used as counting clock.*/ /* Configure the WDG to generate an EOC interrupt each 0.35s */ WDG_DeInit(); WDG_InitStructure.WDG_Preload = 0xFFFF; WDG_InitStructure.WDG_Prescaler = 0xFF; WDG_InitStructure.WDG_ClockSource=WDG_ClockSource_Apb; WDG_Init(&WDG_InitStructure); /* Configure the VIC */ VIC_DeInit(); /* Initialize the VIC*/ VIC_InitDefaultVectors(); /* Initialize default vector registers*/ /* Configure the VIC interrupt */ VIC_Config(WDG_ITLine,VIC_IRQ,0); VIC_ITCmd(WDG_ITLine, ENABLE); /* Enable the VIC */ WDG_ITConfig(ENABLE); /* Enable the WDG interrupt */ /* Enable the WDG in Timer mode*/ WDG_TimerModeCmd(ENABLE); /***********************************************************************/2011-05-17 12:55 AM
hi
1st and just as a remark, do not forget to enable clock to WDT or it won´t work. 2nd, maybe using 91x_scu.c functions, you could get peripheric clock and calc your own time. Take a little look over it, it might help. good luck2011-05-17 12:55 AM
I have configured the WDG clock, and it's working (interrupt generated) at every 0.35second.
Currently i need to genarate an interrupt at an user specified rate. any ideas will be appriciated.2011-05-17 12:55 AM
hi
''from 2, three'' =P or you reprogram WDT to the time interval you wont every time you need to program a diferent one; or you build a couter routine on the WDT ISR routine, wich generate a different software interrupt, where the counter have the N times WDT, needed to generate that other interrupt;(this interrupt could be from a non used EXTINT for example)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.