2003-06-03 10:02 PM
Communication PC, connection between RS232 / I2C by ST72264.
2003-06-02 11:13 PM
Hello!
There is a program in language C to create a communication between the PC and my microcontroleur ST72264. I shall want to exemplify there because I have many of bugs. I found one doc on this site (AN969) but there are no examples of applications. I shall be grateful to you for it if you could help me. I have now create the electronique card, it does not stay in me more than has to bring in the code of the program. I inform you of the evolution of my project. PS: I use the language C and my oscillator is of 8Mhz. Thank you in advance.2003-06-03 5:54 PM
There is source code file available with this application note i.e. AN9zip. I'm here attaching it.
[ This message was edited by: Ranjeet on 04-06-2003 06:35 ] ________________ Attachments : an969.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Ef&d=%2Fa%2F0X0000000bWV%2FEG8Ch6mdf_53lcr2U_u2uEA0y6VhamZUZRRA.I14Xww&asPdf=false2003-06-03 10:02 PM
Hello,
In case you are using STVD7 2.5.2 with the MDT10-EMU3 you need the following patch, available on the net : ''ST72264Gx I2C correction for ST7MDT10-EMU3''.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.