cancel
Showing results for 
Search instead for 
Did you mean: 

Run failed: Error: STM32CubeProgrammer exited with code 1

Kamurasi-Jordan-Arthur
Associate III

Hey there, 
I have run into an issue while trying to using the new edge AI-studio software. I try to make a run such that I am able to the reach the generate project page.

However, currently, I am stack at the point where the pipe running in the EDGE AI studio tries to use the STM32 cube programmer, I think to run the binary and verify it works before proceeding to provide the generated project page.

My set up includes a custom made board, set in DEV boot, and an st-link v3 pwr connected to the custom board. I can confirm that I am able to program the board using cube programmer. I am also able to debug the code programed to this board using XIP paradigm , there for I think the connection there is okay,

The custom boards OCTO XSPI is very similar to that of the stm32n6570.DK as I am able to use the default bootloader for the dev board to be able to program it.

How ever the logs from running the cube AI studio say 

Run failed: Error: STM32CubeProgrammer exited with code 1

I attached a log file to this run as reference.
The very last line in the logs should be the place you are probably looking for. 

I have no communication over USART1 to the virtual com port over USB to on the stlink v3pwr if that's what the SW is looking for to verify if things work.


2 REPLIES 2
Kamurasi-Jordan-Arthur
Associate III

This is just an update.
and just now checking with the STM32N657 Nuecleo board.

I see this log, 
Slightly different but very similar failure, 

My Question, Is the tool only meant to work with the STM32N650-DK. cause I saw another post where they talked about the choice of the bootloader for the Nucleo  not having been put into consideration during the AI studio's SW design at the time.

I cant test with the dev board at the time cause I have had it missed up recently. i.e "wont power up correclty".

Any immediate insight into the matter will save me the project by fur. 

Hi @Kamurasi-Jordan-Arthur,

 

Did you find a solution for your issue? I saw some other post of yours.

STM32Cube AI Studio indeed support the STM32N6, both DK and Nucleo boards.

 

Make sure to update STM32CubeIDE, programmer and cubeMX.

 

Make also sure to be in dev mode when using the N6.
In most of these article, you should find details about how to flash the N6 and the dev mode:

Search - STMicroelectronics Community

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.