2006-03-30 8:32 PM
2006-03-07 11:59 AM
:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armlink --scatter C:\workspace\RDL\STR7_code\common\scat.scf --vfe --ro-base 0x40000000 --rw-base 0x20000000 --first 71x_vect.o
Warning: L6340W: options first and last are ignored for link type of scattered License is dongled to RVI-ME My scatter file looks like this; FLASH 0x40000000 0x8000 { FLASH 0x40000000 { 71x_vect.o (Vect, +First) 71x_init.o (Init) * (+RO) } RAM 0x20000000 { * (+RW) * (+ZI) } }2006-03-07 12:06 PM
in project properties *link advanced does it ignore the Auto via file settings when I have a scatter file defined?
it does not seem to come up with flash memory control when I hit F5 when I have scatter file defined. But seems fine with Auto via file settings.2006-03-08 11:32 AM
Hi RISC,
I want to debug the code using ICE. I must place the code to ext sram 0x62000000.But i found something strangely. When I place the code to cpu sram 0x20000000, It works well. I relink the code to 0x62000000,and download the code to ext sram 0x62000000,It can't run to main function. Another question,You said remap RAM to address 0 ,I have to enable the RAM remapping, therefore uncomment the GBLL remapping and GBLL remap_flash. Why not uncomment the GBLL remapping and GBLL remap_ram? uncomment remap_flash means remap cpu flash 0x400000000 to 0x0000, and does't remap cpu sram 0x20000000 to 0x0000. [ This message was edited by: dom on 09-03-2006 03:05 ]2006-03-09 8:08 AM
ok I wrote some code to copy all the contents from the flash to ram... do I place this code before the GBLL remap? or is it the first instruction before the resethandler?
LDR R1, =FLASHBASE ;FLASH START ADDR LDR R2, =RAMB ;RAM STAR ADDR LDR R3, =RAML ;RAM END ADDR COPY CMP R2, R3 LDRLO R0,[R1],#4 STRLO R0,[R2],#4 BLO COPY well i want to start from flash====>copy to ram=====>remap ram to 0x00002006-03-09 11:27 AM
Hi RISC,
I have enable the EMI Bank 1 using the EMI_config.inc file. I can download the code to EXT SRAM 0X62000000. But It can run to main.2006-03-10 1:20 AM
Hi RISC,
Here is my scat file. I want to download and debug my program to ext sram 0x62000000. I can't go to main function and the debug says ''DBT Warning 00135: Cannot set breakpoints in literal pools'' When i try to step to B __main. I don't what's wrong! When relink the program to cpu sram 0x20000000 It works well.2006-03-10 1:54 PM
Here is my project.
I am using ADS1.2 using ****_cpu_sram to link,the program works well but using ****_ext_sram to link, the program can't go to main. The debug says ''DBT Warning 00135: Cannot set breakpoints in literal pools''. ________________ Attachments : str7.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtBy&d=%2Fa%2F0X0000000aK9%2FQqAFJq0b3I_KzBKNacRIBG0v1SlUYcXdUybHdZY9JCs&asPdf=false2006-03-30 9:49 AM
Quote:
On 10-03-2006 at 09:58, Anonymous wrote: @Dom, could you send me your scatter file. @fixxer, You do not need to copy the code from FLASH to RAM by hand. With an appropriate scatter file the __main will copy the code from FLASH to RAM. Here an example of scatter file: FLASH 0x40000000 0x40000 { FLASH 0x40000000 { 71x_init.o (Init,+First) * (InRoot$$Sections) } RAM 0x20000000 0x10000000 { 71x_vect.o (Vect, +First) * (+RO) * (+RW) * (+ZI) } } In your init.s file you should have the following instruction at the beginning: Reset_Handler LDR pc, =NextInst NextInst NOP NOP NOP : : RAM_remapping B __main Regards. Hi what goes in * (InRoot$$Sections) ? I made some good progress, can boot from flash, but stack pointers seem to get confused, while running from flash.2006-03-30 10:56 AM
This is my MMAP
Image Entry point : 0x40000000 Load Region FLASH (Base: 0x40000000, Size: 0x0000677c, Max: 0x00040000, ABSOLUTE) Execution Region FLASH (Base: 0x40000000, Size: 0x00005db4, Max: 0xffffffff, ABSOLUTE) Base Addr Size Type Attr Idx E Section Name Object 0x40000000 0x0000012c Code RO 412 * Init 71x_init.o 0x4000012c 0x00000008 Code RO 415 * !!!main __main.o(c_a__un.l) 0x40000134 0x00000038 Code RO 470 !!!scatter __scatter.o(c_a__un.l) 0x4000016c 0x0000006c Code RO 468 !!dczerorl2 __dczerorl2.o(c_a__un.l) 0x400001d8 0x00000028 Code RO 472 !!handler_copy __scatter_copy.o(c_a__un.l) 0x40000200 0x0000002c Code RO 474 !!handler_zi __scatter_zi.o(c_a__un.l) Execution Region RAM (Base: 0x20000000, Size: 0x00006294, Max: 0xffffffff, ABSOLUTE, COMPRESSED[0x000001d8]) Base Addr Size Type Attr Idx E Section Name Object 0x20000000 0x000004c0 Code RO 405 * Vect 71x_vect.o2006-03-30 1:16 PM
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.