2011-04-19 12:39 PM
Hello,
I want to use the beep function with my STM8L Discovery. After writing the program to STM8L, I connect the a piezo speaker between PA0 and GND. The program is as following: // Initialize BEEP_LSICalibrationConfig(16000000); BEEP_Init(BEEP_Frequency_1KHz); //Beep BEEP_Cmd(ENABLE); delay_ms(200); BEEP_Cmd(DISABLE); But it doesn't work. Do I need something another command on Initialization process ? I know the PA0 is connected to the SWIM. Is it affect something bad for the beeper function?2011-06-01 2:46 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.