Replacement for START499TR part
Hello Team,Please suggest the replacement for START499TR part.Early response is highly appreciated.Thanks and Regards,Rakshitha
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello Team,Please suggest the replacement for START499TR part.Early response is highly appreciated.Thanks and Regards,Rakshitha
我使用 X-CUBE SAEFA1 在 stm32l151 上的 STSAFE-A110 中运行身份验证例程,串口返回 6 或卡住,寻求帮助
Hii, I was trying to run bldc motor using STEVAL-SPIN3202 evaluation board using 6-step method but i am unable to rotate the motor. When i press the start button it rotate just the fraction and overcurrent , speed feedback error is shown in motor pil...
Hi I am a new user, Can any please tell me which software do I need to use for STEVAl STRKT01? My aim is to transmit lora signal and received this signal on spectrum analyzer.
I have a new design that uses an STM8L151 and I was wondering if the STM8S/A Standard peripheral library can be used to design the code for it.I do realise that at least the stm8s.h should be modified, but can it be used at all?
Posted on January 09, 2017 at 10:00 So, info in reference manual is irrelevant? The read should be always done as: ; Read Seq_1 ld A, TIM1_REGH; ld XL, TIM1_REGL;�?�?�? ? Will the following sequences lead to incorrect results? ; ...
I am trying to program the STM8S001J3 microcontroller, on a custom board. I am using ST Visual Programmer tool for flashing the program but I’m running into the following error continuously.I have tried using both ST-Link/V2(A) and ST-Link/V2(A) ISOL...
When using the chip GIPS30C60-H, a 10k pull-up resistor is used to set SD/OD high and the CIN pin is directly grounded, but there is no three-phase output voltage when the correct pwm signal is input. The chip is used in a motor controller and has a...
Hi, We are using 54AC164245 device for our onboard application. We have connected VDD1 as 5V and Vdd2 as 3.3V. As per datasheet the side A side max input voltage allowed is <=Vdd2. In the case when the device will be in disable condition (Isolation) ...
Hello community,I'm looking for materials to learn STM8S programming.I searched on the internet but I couldn't find anything. Can you recommend me any documents or links to learn, please?Thank you all!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.