Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EEPROM content erased - M24M01-RMN6P

Hi,Currently, I am using EEPROM (p/n:M24M01-RMN6P) for data logging.The chip is operating at 3.3V and the circuit shown in the figure below.An incident happened that the EEPROM content has been erased and when we read back the contents of the EEPROM,...

HW001 by Associate II
  • 6111 Views
  • 10 replies
  • 4 kudos

stm8s flash entire new program - how?

Let's assume I have a program that exposes a serial interface for commands and one such command is "load new program".  I upload the new program as hex strings and the old program writes this to flash and the resets.  Hopefully at this point the new ...

Resolved! Does ST-Link/V2 support STM8S103F3 ?

Dear All,I started working on the STM8S Mcu's recently. Here I have some basic queries.1)By using this ST-Link V2 in circuit debugger and programmer. (ST-LINK/V2 - ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32 - STMicroelectronics) Can...

Halt mode and Current consumption

Hi, I have a STM8S001J3. I want to put my uC in halt mode because I'm on battery. The problem is that halt mode consume around 1mA when the interrupts are enabled. I need interrupts to wake up from halt mode with my GPIO pin so I can't disable it.I t...

MSL

Hello , Is it possible that I have MSL 1 on a label even though everywhere else says that this Part is MSL 3?

Diwo72 by Associate
  • 1383 Views
  • 1 replies
  • 0 kudos

USB Power Delivery using STUSB1602 library

Hi there,We are using the STUSB1602 for charging 10W devicesI'm looking to download the STSW-STUSB010 library, It seams that the STSW-STUSB010 library is not available, also from web search, there is version 015  some sites claim that the library is ...

GalBTM by Associate II
  • 2331 Views
  • 3 replies
  • 0 kudos

LittleFS with M95256-DRMN3TP EEPROM Device

Hello, I am using M95256-A125 EEPROM device as NV data storage in our application. SPI communication is used to communicate from host to EEPOM device. EEPROM  Device has page size 64bytes but little-fs expects minimum page size as 104 bytes.  My ques...

Dev001 by Associate
  • 870 Views
  • 0 replies
  • 0 kudos

Resolved! diode reference BUZ GP642 or BUZ Z338

 Bonjour à tous, quelqu'un pourrait m'aider à trouver la référence de cette diode ou un équivalent, car je ne trouve pas la fiche technique sur internet, je vous remercie d'avance pour vos réponses 

IMG_20241125_150332.jpg
MAOU by Associate
  • 2364 Views
  • 3 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.