2024-07-29 7:58 AM
Hi,
I have a STM8S001J3. I want to put my uC in halt mode because I'm on battery. The problem is that halt mode consume around 1mA when the interrupts are enabled. I need interrupts to wake up from halt mode with my GPIO pin so I can't disable it.
I tried without the interrupts and the current consumption is around 4uA.
I can't imagine that interrupts consume so much and that this issue is mentionned nowhere in the documentations.
I join here a copy of my main function:
main()
{
GPIO_Init (LED, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_Init (BT, GPIO_MODE_IN_PU_IT);
GPIO_Init (GPIOA, GPIO_PIN_3, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_Init (GPIOD, GPIO_PIN_6, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_WriteLow(GPIOA, GPIO_PIN_3);
GPIO_WriteLow(GPIOD, GPIO_PIN_6);
EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOB, EXTI_SENSITIVITY_RISE_ONLY);
enableInterrupts();
while (1)
{
if (bouton() && oneTime) //if button pressed
{
oneTime = 0;
if(sleep)
{
sleep = 0;
}
else
{
ledOff();
sleep = 1;
halt();
}
}
else if(!bouton() && !oneTime)
{
oneTime = 1;
}
}
}
2024-11-29 2:59 PM
Hello,
Make sure all IOs are in some defined state. i.e. do not leave any IOs floating. either set them to output, add pull up/down external resistor or enable the internal pull up resistor.
The analog front end of the gpio will consume power when a floating voltage wiggles about.
If I recall correctly only the stm8l* parts have ultra low power mode that achieves < 1 uA in the most extreme halt mode... just in case that is what you are trying to achieve.
see https://community.st.com/t5/stm8-mcus/cannot-enter-low-power-mode-stm8l052c6/td-p/356194
the stm8s001j3 datasheet shows 4.5uA typical @ 3.3v in HALT mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.