2008-08-12 1:22 AM
2008-08-07 11:34 PM
Hi.
I'm trying to learn Cosmic Compiler program. For programming ST7 microcontrollers. I have a problem about Compile and build. I work with example program. I press compile or build button and i get this error message ''Can't Access File:IDEABLD.BAT in Project Directory. Check Access Rights.'' I use Windows Vista as operating system. Could you help me. Thanks. Burak Akçasu.2008-08-10 8:23 PM
2008-08-11 6:59 PM
Quote:
On 11-08-2008 at 08:53, Anonymous wrote: as the error message says, make sure you have full rights on the project directory. If you have no clue, log in as admin and try again. Regards, Luca (Cosmic) Thanks for your answer. But it didnt work. I have full rights on project directory but still i get same error message. I think it is about Windows Vista. Thanks again. I think i must return Windows XP :).2008-08-11 10:46 PM
2008-08-12 1:22 AM
thanks.
2011-05-17 6:31 AM
Hi, I saw the posted problem but didn't see solution.
Could anybody help? I work with example program. I press compile or build button and i get this error message ''Can't Access File:IDEABLD.BAT in Project Directory. Check Access Rights.'' I use Windows-7 64bit as operating system.2012-01-11 5:27 PM
you should use 32bit system.
2012-01-23 12:29 AM
Hi,
I failed to start the Cosmic Compiler when residing the source files on our intranet. After I've transferred all my files to my local drive - there has been no problems any more. Take it just as a suggestion, WoRoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.