Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

use rs232 uart with stm8l discovery board

Posted on August 12, 2011 at 01:06Hi, I would like to use the uart device of the stm8l chip on the stm8l discovery board. I notice that uart and cristal are shared on the same pins (PA2 and PA3) Do you think it is possible to use the uart when the s...

pub by Associate
  • 941 Views
  • 1 replies
  • 0 kudos

Instruction Trap 0x83

Posted on May 03, 2013 at 18:38Hi. I have a program in STM8L152R8, my firmware has a size of 0xEFE1. I want to prevent that for any reason my microcontroller work bad. So, I want to fill  the rest of the hex file (0x901E) with 0x83 (interrup trap). ...

prueba2 by Associate II
  • 1087 Views
  • 2 replies
  • 0 kudos

ROP and bootloader

Posted on June 27, 2012 at 18:20Hi,Does anybody knows how to jump properly to Bootloader entry point at adress 0x602D?I 've tried :#define BOOTLOADER_ADDR 0x602Dultypedef  void (*TFunction)(void);void JumpToBootLoader(void){const TFunction MainUserA...

jfelix by Associate II
  • 3063 Views
  • 9 replies
  • 0 kudos

How to change __iar_program_start address

Posted on March 05, 2013 at 08:10Dear all, i want to set '' __iar_program_start ''  in the absolute address(ex:0x9100). so, i am setting override default program entry and entry symbol is '' iar_reset ''. and program is: #pragma location = ''.CallBa...

ellisshz by Associate II
  • 1545 Views
  • 1 replies
  • 0 kudos

ride7 and STR91x_Lib

Posted on May 08, 2013 at 22:51hi to all. can't get lib to work, tryed GPIO example but it did not worked on real mcu, tryed  in simulation mode where i see default value of registers, i've tryed example as is, without any changes.can't say version ...

khorght by Associate II
  • 855 Views
  • 0 replies
  • 0 kudos

bcd to bin

Posted on April 30, 2013 at 09:19hello, please can help me someone one with an assembly language  who convert a 5digit BCD to BIN many thanks

EEPROM Write Timing Problem

Posted on April 16, 2013 at 14:18Hi, I found a problem while writing to the EEPROM. The uC type is STM8af6289. This part of the program is the folowing: initializing part: void FLASH_Config(void) {     FLASH_SetProgrammingTime(FLASH_PROGRAMTIME_STAN...

Problem with STDV-Cosmic compiler

Posted on February 05, 2013 at 04:46I am a newbie at cosmic and I met something strange when using STVD with cosmic compiler to run my project. I hope that somebody can explain it for me. This is my project: It is my main: &sharpinclude ''peripheral...

Storing some calibration data in FLASH memory

Posted on April 17, 2013 at 22:32Hello, I'm looking into storing some calibration data for my application into FLASH memory since my EEPROM space is very valuable and I cannot spare any of it. The cal data would only be written once (upon the first ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.