2013-05-03 9:38 AM
Hi.
I have a program in STM8L152R8, my firmware has a size of 0xEFE1.
I want to prevent that for any reason my microcontroller work bad. So, I want to fill the rest of the hex file (0x901E) with 0x83 (interrup trap).
in my programm I have the next code (main.c):
void vFill_Trap(void)
{ &sharpasm switch .textdcb.b 36894, $83 ; allocate trap bytes
; all initialized to $83&sharpendasm
}I need the main.c file be the last to compile.
How I can do this?
I use the STVD and Cosmic.
Thanks.
#trap-interrup-0x83-fill-hex2013-05-07 5:36 AM
I'm not sure what you are really trying to do but if you just want to specify the compile order, you can do that very simply. The order in which the source files are compiled is the order in which they appear in your ''workspace project'' folder. Follow the directions outlined in the STVD help manual in section 3.6 ''Ordering source files before assembly.'' Here is what it says:
Project > Insert Files Into Project
)Add Sorted Elements
option in the project contextual menu.Add Sorted Elements
option in the project contextual menu.2013-05-13 1:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.