Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S - Discovery - Touch Library Problem

Posted on June 03, 2013 at 15:44Hello,I am actually working on a project based on the Touch RC Acquisition.I have downloaded the example from the ST website, but I didn't understand why the acquisition pin is wired on Timer 1 while according the STM...

loic by Associate II
  • 1125 Views
  • 2 replies
  • 0 kudos

RTC Clock 'hello world' program STM8L cpu

Posted on June 30, 2013 at 13:07Can anyone help with some code to use the RTC clock as a clock. I'm using the STM8L-Discovery board and not sure how to set the chips registers and to set / read time to the LCD display. I just need a 'hello world' pr...

Active/Halt wakeup with RTC

Posted on May 03, 2013 at 14:36Hi ,I am a new user of STM8.  In my project I am using Active/halt mode an it wakes up with RTC Wakeup operation. My problem is, it is always waking up same times. it's equal to 3ms. I want update auto wake up times. I...

Routing Interface (RI)

Posted on May 07, 2013 at 14:58I am using the STM8L151C6T6. I would like to route PD6 to TIM1 Input Capture IC2. The following code executes but does not change the RI_ICR1 register value and the routing does not take place either.     GPIO_Init(POR...

wynand by Associate II
  • 1129 Views
  • 1 replies
  • 0 kudos

COSMIC LKF File

Posted on May 27, 2013 at 11:48Hi All, I want to execute some command in .lkf file for COSMIC Compiler condionally. is it possible?? Pseudo code is as below: /*--------------------------*/ #ifdef TRUE obj\libisl.sm8 #else obj\libis0.sm8 #endif /*---...

Storing some calibration data in FLASH memory

Posted on April 17, 2013 at 22:35Hello, I'm looking into storing some calibration data for my application into FLASH memory since my EEPROM space is very valuable and I cannot spare any of it. The cal data would only be written once (upon the first ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.