Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Virus in the Cosmic compiler?

Posted on July 18, 2013 at 15:34I have domnloaded the free Cosmic Compiler STM8 32K and installed it. My AVG Antivirus program reports a trojan horse ''FakeAlert.NT'' in the file cvdwarf.exe (used in the Cosmic software). Have anybody experienced th...

nd by Associate
  • 1102 Views
  • 1 replies
  • 0 kudos

STGIPL14K60

Posted on July 19, 2013 at 06:07I bought STGIPL14K60 ..I want to rectify the 3 phase input. When i rectify it , I got about 585VDC.  Can i connect this high voltage to the MODULE or not. #edesignsuite #pfc #power-supply #rectifer #dc-chopping #s...

0690X00000605dMQAQ.png
saraaj100 by Associate II
  • 2849 Views
  • 4 replies
  • 0 kudos

Looking for an MCU reference

Posted on July 23, 2013 at 10:24Hi all,I had good experiences on STM32F4 peripherals, but I'm new to ST 8 bits family, so I'd like your feedback and help to match a good MCU at lower cost possible, and that could match that features :- 3.3V operatio...

neoirto by Associate II
  • 2078 Views
  • 4 replies
  • 0 kudos

ST7540

Posted on March 11, 2013 at 16:26Hi, i use the ST7540 and got the problem, that the demodulated bits are shifted sometimes, because of first bit is lost. How can i solve this problem? And where can i find more information about extended control regi...

crused by Associate
  • 1365 Views
  • 1 replies
  • 0 kudos

Mistake in the STM8L15xx8 Datasheet

Posted on July 23, 2013 at 00:08I use the STM8L152M8 to drive a complex LCD. In the datasheet (Doc ID 17943 Rev 5), page 35, it is written: for PIN 52...56 (PF4...7): LCD_SEG36...39. In the reference manual (Doc ID 15226 Rev 10),  page 267, ''the SE...

pascal by Associate
  • 815 Views
  • 0 replies
  • 0 kudos

ST6 Controller Toolchain or IDE

Posted on July 22, 2013 at 08:28Hello,  i would like to download the ST6 Assembler-Linker Toolset (PN: STSW-ST6005) from your internet location. Link : http://www.st.com/web/en/catalog/tools/PF257578 But unfortunately there is no file to download. I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.