Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Urgent: STM8S003F3 reset pin gets damaged

Posted on December 05, 2014 at 14:58I am using STM8S003F3 & attached is circuit. I have connected some switches in pull-up configuration as shown. After some correct operations, I have seen that some of boards stopped working. It was problem 1 as ...

STM8L Interrupt

Posted on October 29, 2014 at 17:07Hello, I'm using the STM8L151 using IAR workbench without ST Firmware Library and I'm trying to use an SPI Interrupt. Unfortunatey it doesn't work. SPI is already running, the receiving flag is set, but i don't get...

ST7540 Eval Board SPI ( urg )!!!!!

Posted on May 22, 2013 at 11:22Hi , I'm using ST7540 Eval Board and i want to send to my Micrcontroller via SPI , 24 bits all at once. The spi i use is 8 bit. Here is an excerpt of my code : volatile uint8_t i=3;     while(i>0){         i--;        ...

elazhar by Associate II
  • 1268 Views
  • 1 replies
  • 0 kudos

STM8 Evaluation- Independent watchdog

Posted on December 01, 2014 at 08:15Hello,  According to reference manual IWDG will not be stopped even after entering HALT mode. Is there a possibility to STOP or PAUSE IWDG for STM8A ? According to STM8AL we can halt IWDG, but STM8AL is not suitab...

kawasthi by Associate
  • 853 Views
  • 0 replies
  • 0 kudos

Active halt low power mode

Posted on November 11, 2013 at 12:34HiWe are developing with STM8L152C6 microcontroller and debugging using the discovery board.Our application uses a battery when there is no power. In this case, we need only two I/O interrupts and the LCD to be wo...

design by Associate
  • 2255 Views
  • 3 replies
  • 0 kudos

STM8S105 2 channel ADC1 problem

Posted on November 20, 2014 at 11:41Hi AllI want to read 2 channel ADC from ADC1 library. You can see my code below. I used scan mode and conversation mode single. I take 4 samples in interrupt and used average of them in my main code. My problem is...

idurgun by Associate
  • 928 Views
  • 0 replies
  • 0 kudos

ESM7045DV datasheets

Posted on November 09, 2014 at 03:21Dear all, I had been trying really very hard to search by internet and or trying to call ST distributor searching for DATASHEETS of ESM7045DV, unfortunately I found nothing.Is there anyone that could help me out p...

hongya_li by Associate II
  • 1706 Views
  • 2 replies
  • 0 kudos

STM8 SWIM pin as output/Debug

Posted on November 08, 2014 at 11:361. I have STM8S003F3 & want to use its debug pin as output. So I will configure it my code.2. Will that make debug option dead?On next power up, will I be able to debug the code?? Because pin will already be confi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.