2014-11-20 2:41 AM
Hi All
I want to read 2 channel ADC from ADC1 library. You can see my code below. I used scan mode and conversation mode single. I take 4 samples in interrupt and used average of them in my main code. My problem is sometimes ADC1_GetBufferValue(1) or ADC1_GetBufferValue(0) returns bigger than 1023. For example 20000, 40000 or something like that. Could you have any opinion for this issue ?void ADC_Configuration(void){ ADC1_DeInit(); ADC1_Cmd(ENABLE); ADC1_Init(ADC1_CONVERSIONMODE_SINGLE, ADC1_CHANNEL_1, ADC1_PRESSEL_FCPU_D18, \ ADC1_EXTTRIG_TIM, DISABLE, ADC1_ALIGN_RIGHT, ADC1_SCHMITTTRIG_ALL, DISABLE); ADC1_ScanModeCmd(ENABLE); ADC1_ITConfig(ADC1_IT_EOCIE, ENABLE); ADC1_DataBufferCmd(ENABLE); ADC1_StartConversion();} INTERRUPT_HANDLER(ADC1_IRQHandler, 22) { ADC1_ClearITPendingBit(ADC1_IT_EOC); //ADC1_ClearFlag(ADC1_FLAG_EOC); wBATTERY_VOLTAGE_SUM = wBATTERY_VOLTAGE_SUM + ADC1_GetBufferValue(1); byBATTERY_VOLTAGE_SAMPLE_COUNT++; if(byBATTERY_VOLTAGE_SAMPLE_COUNT > 3) { wBATTERY_VOLTAGE = wBATTERY_VOLTAGE_SUM>>2; wBATTERY_VOLTAGE_SUM = 0; byBATTERY_VOLTAGE_SAMPLE_COUNT = 0; } wBOOST_VOLTAGE_SUM = wBOOST_VOLTAGE_SUM + ADC1_GetConversionValue(); byBOOST_VOLTAGE_SAMPLE_COUNT++; if(byBOOST_VOLTAGE_SAMPLE_COUNT > 3) { wBOOST_VOLTAGE = wBOOST_VOLTAGE_SUM>>2; wBOOST_VOLTAGE_SUM = 0; byBOOST_VOLTAGE_SAMPLE_COUNT = 0; } } #adc1 #stm8sWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.