Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External interrupt with ir sensor

Posted on June 26, 2015 at 15:27Hello I m trying to generate a interrupt using ir output but external interrupt is not responding.Im using stm8s003f3 and stvd .And it do respond with external interrupt as switch .  EXTI_SetExtIntSensitivity(EXTI_POR...

ekta by Associate II
  • 992 Views
  • 1 replies
  • 0 kudos

Stm8L custom bootloader vector table.

Posted on July 07, 2015 at 16:30HiI wrote custom bootloader for stm8l152c8. Its working fine. But i want to write two user application to the board. For example i have 2 application one of them is starting 0x9000 other one starting 0xB000 adresses i...

emre2 by Associate
  • 1142 Views
  • 1 replies
  • 0 kudos

Need help

Posted on June 24, 2015 at 15:40Hello can anyone provide me email id for support team for stm microcontroller . Please reply.. #stm

ekta by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos

ST-LINK/V2 Documentation

Posted on June 26, 2015 at 12:49Hello,we do not use Windows as development / build platform and have now a STM8L device in our project that we would like to flash during development. Using some official ST supported flash tool under windows for prod...

torsten2 by Associate II
  • 1412 Views
  • 2 replies
  • 0 kudos

EEPROM invalid values

Posted on June 24, 2015 at 09:04Hello, I'm pretty new in STM8 programming. I'm making small project on STM8S103F3P6 microcontroller and I need to save some (27 bytes) values in EEPROM memory and reload them at every power up. I saw an example from S...

STM8 I2C Busy Bit is always 1

Posted on April 28, 2015 at 11:00Hello, I work with the STM8S105K6 and have tried several examples of ST here. SDA and SCL have a 4.7K pull-up. The line is currently connected only with a oscilloscope. Manually I can let toggling the corresponding...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.