ST10
Posted on September 22, 2015 at 12:57ST10
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Posted on September 22, 2015 at 12:57ST10
Posted on April 08, 2014 at 16:53Maybe some of you with SPI experience can spot this one easily. I have a SPI slave device connected to my STM8L152. I watch the clock and data stream to the device requesting a read of a register, and then I can see ...
Posted on September 14, 2015 at 15:06Hello everybody, in my Cosmic C program for a STM8S003 I have a problem: The result of some floating point calculations are sporadically corrupted. The usage of variables can not be the cause for that because the...
Posted on September 10, 2015 at 16:47 Hi, I am trying to read the Flash protection registers using something like the following: #define FLASHPR_BASE 0x8010DFB0 #define FLASH_NVWPR ((volatile uint32_t*)(FLASHPR_BASE + 0)) #...
Posted on September 10, 2015 at 07:26 hello, I've been trying to blink an led using an overflow interrupt with timer 4 on the sm8l discovery board. So far I haven't made it work. I'm currently using IAR Embedded Workbench with the Std lib...
Posted on September 07, 2015 at 12:00how to use 64 bit data type in stm8s003f3? if i use unsigned long long its not takeing and giving error. #st
Posted on September 06, 2015 at 17:28 Hello all, I'm stuck for a long time without results. (I'm using STM8S105C6 discovery with IAR IDE) I'm trying to measure a pulse time in one of 2 ways: 1. Manually, by starting the timer when t...
Posted on August 17, 2015 at 21:48My first project using the tool eDesignSuite and I'm developing a switching power supply with a 85VAC to 265VAC input voltage with 24VDC output and 5A of output current. My difficulty is in finding the transformer t...
Posted on September 01, 2015 at 06:03do we have any c code for keeylog decryption ? #keeloq-algorithem-for-stm8---stv
Posted on August 30, 2015 at 01:49 I'm at my wit's end, I cant seem to make SPI receive work properly. This is a cut from the S003 reference manual: This is the capture from the logic analyzer: And this is th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.